Cable assemblies
Cable assemblies
Cable assemblies are cables that are factory-fitted with one or two connectors at the open ends. They are ready to connect directly, save time, streamline internal processes and fulfil the highest quality criteria due to LAPP''s expertise. Our portfolio includes various power and control cable assemblies and different data network cable assemblies.
What is a cable assembly or an assembled cable?
A cable assembly is a ready-to-connect cable that has already been fitted with a connector at one or both ends. An assembled cable is ready for use immediately and can be connected directly at the intended location. Process steps, which are sometimes time-consuming, such as stripping the cable, stripping the cores, crimping the conductor and final connector assembly that would otherwise occur on site are completely omitted.
Cable assemblies are not only produced in the factory by a cable manufacturer, but are also thoroughly checked. Standardised production steps ensure that cable assemblies meet the same quality criteria. Unlike cables that can be assembled by ourselves, there are considerably fewer errors during assembly by experienced employees in semi-automated production steps and with high quality requirements.
Quick view AB-C8-M12MA-[L]PUR
Article No.: 22260094
Quick view AB-C8-M12MS-[L]PUR
Article No.: 22260093
Quick view AB-C8-M12MS-[L]PUR
Article No.: 22260092
Quick view AB-C8-M12MS-[L]PUR
Article No.: 22260091
Quick view AB-C5-[L]PUR-M12FA-3L
Article No.: 22260416
Quick view AB-C5-[L]PUR-M12FA-3L
Article No.: 22260409
Quick view AB-C5-[L]PUR-M12FA
Article No.: 22260418
Quick view AB-C5-[L]PUR-M12FA
Article No.: 22260407
Quick view AB-C5-[L]PUR-M12FA
Article No.: 22260406
Quick view AB-C5-[L]PUR-M12FS
Article No.: 22260415
Quick view AB-C5-[L]PUR-M12FS
Article No.: 22260405
Quick view AB-C5-[L]PUR-M12FS
Article No.: 22260404
Quick view AB-C5-M12MS-[L]PUR
Article No.: 22260400
Quick view AB-C5-M12MS-[L]PUR
Article No.: 22260414
Quick view AB-C5-M12MA-[L]PUR
Article No.: 22260403-