Skip to content
LAPP Malaysia
Spend RM200 MYR more for FREE shipping.
FREE shipping will be applied at checkout

Your cart is empty

Continue shopping
0 Cart (RM0.00 MYR)

Pre-Assembled Harnesses for Data Centre Rack Power Distribution

AI-generated industry illustration. No LAPP products depicted.

How many hand-made terminations sit between a new data hall and its first live rack? On a build running a few hundred racks, the count runs into the thousands. A pre-assembled rack power harness is a cable and connector assembly built and tested to length in the factory, then installed as one unit rather than terminated by hand on site. That moves the error-prone part of the job off the critical path and off the live floor, and it leaves a documented bill of materials for every run instead of a connection nobody tests until power is on.

Our data centre cabling guide already covers which power and network cables a high-density rack needs, from the PDU through to the patch panel. This piece takes that selection as settled and looks at the layer above it: whether to buy those rack power runs as factory-assembled harnesses or terminate them by hand on site. We made the same argument for machine builders a while back. The data centre version has a different pressure behind it, which is schedule.

Why does field-terminating rack power distribution slow down data centre builds?

Because termination is a skilled, serial task, and a rack power build has a great deal of it. Every rack takes a feed, every feed needs a connector at each end, and on a field-terminated job each one of those is made by hand at the rack by an electrician who can only be in one aisle at a time.

That work also lands late. Racks are in place, the power path is energised, and the programme expects the runs to appear in a window that has already absorbed whatever slipped upstream of it. Termination is usually the trade with the least slack left when its turn comes.

Repeatability is the second cost. Hundreds of racks want the same run length and the same connector orientation so the aisle stays tidy and the airflow stays predictable. Hand-made runs drift, crew to crew and rack to rack, and the drift shows up in cable management long after the electrician has left.

Then there is the joint itself. A field crimp is made once, under site conditions, and its quality rests on the crew and the site QA that day. A loose one can pass inspection and still be the reason a rack drops months later, on live equipment, which is the most expensive place in the building to find it.

Documentation is the quiet one. Hand-terminated runs are recorded as well as the crew on that shift recorded them, and handover packs vary accordingly. A build-to-print harness ships against a defined bill of materials, so what was installed is auditable without going back to the aisle to look.

What should a pre-assembled harness for rack power distribution include?

Start with the length. A harness is a build-to-print item, so the run length, the connector at each end and the orientation are fixed in the drawing before anything is cut. That drawing is the thing the factory builds to and the thing site installs against, and getting it right is most of the work.

Cables and connectors get specified together here, not bought separately. For rack power distribution that is typically LAPP ÖLFLEX® power and control cable with EPIC® connectors, chosen against the actual rack and PDU interface. Confirm the exact type and rating against LAPP before it reaches a bill of materials, rather than treating a general article as the specification.

A test record belongs in the package. The point of a factory-assembled harness is that it was made under production conditions with the same tooling every time and tested electrically as a finished item before it shipped. If that record does not come with the harness, half the argument for buying one has gone.

Labelling and packing sequence matter more than they sound. Harnesses that arrive labelled to rack position, and boxed in the order the aisle gets built, turn an install into a sequence anyone can follow. Harnesses that arrive as a pallet of identical bags put the sorting back on site.

One reason the harness is worth buying as a single item is that LAPP designs and manufactures both the cable and the connector, and assembles the two into the finished harness. That keeps the cable, the termination and the test record with one manufacturer, which is a shorter path than sourcing the parts separately and asking site to make them agree.

Two things sit outside a harness scope, worth saying plainly. The rack power and network cable selection itself is covered in the cabling guide and in our piece on powering GPU racks. IT and network fabric assemblies, the copper and fibre patch between switch and server, are a separate conversation, and busway or busbar distribution stays with the electrical contractor rather than with the cable and harness scope.

How do pre-assembled harnesses change data centre commissioning timelines?

They change what happens in the last window before handover. Field termination puts make, inspect and test inside that window. A pre-assembled harness has already been made and tested weeks earlier, in a factory, against the same drawing, so the site task reduces to route, connect and check.

Testing moves earlier too, which is the part that tends to get underestimated. A fault found on a production line is a rebuilt assembly. The same fault found at commissioning is a crew back in a live hall, working around equipment that is already energised, against a date that has stopped moving.

Picture a colocation hall going in a few hundred racks at a time, with the mechanical trades still on the floor and a customer move-in date fixed. Field-terminated, the power runs are a task that cannot start until the racks land and then moves at the pace of the crew. Pre-assembled, they are a delivery scheduled against the rack sequence and an install that keeps pace with it.

Handover gets easier at the same time. Every run has a drawing, a bill of materials and a test record behind it, so the commissioning pack is assembled rather than reconstructed. That is also what makes the next hall cheaper to specify, because the drawing set already exists.

How much of this pays back varies with the build. A dozen racks in an existing hall will not move a programme either way. Several hundred identical racks on a compressed schedule is where the arithmetic changes, and that is the case worth putting numbers against before the crews are booked.

Talk to Our Engineers

If you are pricing rack power distribution for a build and want to compare pre-assembled against field-terminated properly, the useful next step is a conversation about the actual rack interface rather than a catalogue page. Send the drawings and the rack count, and our connectivity specialists can work through the cable, the connector and the harness build with you.

The details that shorten that conversation are the rack and PDU interface at each end, the run lengths and how many of each, the rack count and build sequence, the containment and routing in the aisle, and the date the first racks need power. Those five turn a general enquiry into a build-to-print drawing.

Talk to our connectivity specialists through the LAPP SEA enquiry page and ask for the data centre infrastructure channel. For the harness scope itself, start from LAPP Harnessing Solutions and the cable assembly range, or the download centre for current catalogues.