Skip to content
LAPP Malaysia
Spend RM200 MYR more for FREE shipping.
FREE shipping will be applied at checkout

Your cart is empty

Continue shopping
0 Cart (RM0.00 MYR)

LAPP Harnessing Solutions: Pre-Assembled Connectivity for Hygienic Machine Builds

AI-generated industry illustration. No LAPP products depicted.

A hygienic machine build benefits when its cable, connector and gland are assembled and tested together against the machine builder's specified requirements, rather than sourced separately and built up on the shop floor. LAPP Harnessing Solutions supplies that as a build-to-print harness, with the drawing, the applicable tests and the record package agreed for that assembly as project deliverables. The hygienic validation of the finished machine, and its factory and site acceptance, stay with the OEM and its customer.

The cable-side decisions for a food or beverage line are covered in Reliable Cable Solutions for Food and Beverage Applications, and the general make-versus-buy question is covered in Outsourcing Cable Harnessing. This piece sits where those two meet: what changes in the specification once the harness has to survive washdown or clean-room duty, and what its records are actually worth at commissioning.

Why does an in-house wiring harness cost more than it looks like on the shop floor?

The visible cost is the labour hour. Someone routes the cable, terminates each connector, fits the gland and dresses the loom, and that hour lands on a timesheet where anyone can see it. It is usually the only number that gets counted.

The less visible cost sits in what that hour is taken from. An hour a design team spends hand-terminating a harness is an hour off the machine's differentiating engineering, and unlike a one-off tooling cost it scales up with production volume instead of shrinking as the platform matures. As an illustration, a builder shipping the occasional one-off can often absorb that. A builder standardising a platform across variants usually finds it harder to.

Then there is the rework tail. Each hand termination is another chance for a mismatched IP rating, a mis-seated connector or a gland fitted outside its assembly instructions, and on a hygienic machine those are the faults that surface late. A bad seal found at a wet test or a customer audit costs more to reach than the termination ever did.

Consider a packaging-machine builder standardising a wash-capable variant across three frame sizes. This example is hypothetical, but the shape of it comes up again and again: three slightly different shop-floor builds, each documented informally, each depending on who was at the bench that week. The per-unit labour line looks affordable. The variation between units is the part that shows up during commissioning, and a single specified, repeatable harness exists to take that variation out.

The general case for pre-assembly is set out in LAPP Harnessing Solutions: Pre-Assembled for OEM Scale. What follows is the part of that argument specific to hygienic duty.

What changes in a harness spec for a hygienic or washdown machine?

On a general machine, a harness specification can lean on the individual component ratings and assume they add up. On a hygienic or washdown machine, the cable, the connector and the gland are better treated as one assembly checked together against the machine builder's stated requirements, rather than as three parts assumed to behave as a system once they are joined.

Cleaning duty is the reason. Washdown and clean-in-place routines apply high-pressure water and, on many food, beverage and pharmaceutical lines, caustic or acidic agents on a fixed cycle. A connector rated for general dust and splash can hold on a dry bench and still fail at the seal after repeated wet cycles, which is why the sealing interface and the gland entry get specified deliberately instead of inherited from a catalogue default.

The components are the familiar ones: EPIC® connectors at the interface, ÖLFLEX® cable for the run and SKINTOP® glands at the entry. What matters is not the brand list but the pairing, and the exact variants. Their ratings and their suitability for a given cleaning regime belong on the product datasheet and, where the agents are aggressive, in a written confirmation for that chemistry, because an IP water-ingress rating speaks to water under a defined test and not to chemical durability or surface cleanability.

Version control is the quieter change. A late design swap, a different connector or an added sensor, is easier to manage against a controlled harness drawing and bill of materials than against an undocumented shop-floor build, because the change lands in a document that already exists rather than in somebody's memory of how the last one went together.

The table below separates duties that are easy to blur on one specification sheet.

Harness aspect What it addresses What it does not address
IP water-ingress rating on a component Resistance to water ingress under that rating's defined test Chemical durability against the cleaning agent, or surface cleanability
Sealing interface chosen for the cleaning duty Holding the seal across repeated wash or clean-in-place cycles The machine's hygienic zoning or process design
Harness assembled and tested as one item Cable, connector and gland verified together against the agreed specification Validation of the finished machine's hygienic compliance
Version-controlled drawing and bill of materials Traceable change control on the harness itself OEM and customer acceptance of the machine

LAPP Harnessing Solutions builds fully assembled and quality-tested harnesses to the machine builder's own specification, as the LAPP Harnessing Solutions overview describes, and the regional harnessing page sets out how that work is scoped locally. Read it as a build-to-print harness with agreed tests and records for that project, not as an open-ended promise that every assembly carries every conceivable test.

How does a pre-assembled harness change FAT and SAT for a machine builder?

Factory and site acceptance testing are where a machine builder proves the machine to its customer, and both lean on documentation. When the harness arrives with the test records that were agreed for it, those records become evidence the builder can fold into the acceptance file instead of reconstructing after the fact. Our connectivity checklist for commissioning covers the wider set of checks that sit around them.

The distinction worth keeping straight is what those records cover. They attest to what the OEM and LAPP agreed for the harness: continuity, the specified seal checks and whatever else was written into the project deliverables. They do not stand in for the machine's own validation, and acceptance of the finished machine remains the OEM's and the customer's to run and to sign.

That boundary is a feature rather than a gap. LAPP supplies a documented, repeatable harness into the OEM's machine design. The OEM keeps the machine validation and the hygienic sign-off, because both depend on the whole machine and its process rather than on the wiring alone. Framed that way, the harness records support acceptance without ever claiming to certify the machine.

For a builder standardising across variants, the practical payoff is repeatability at commissioning. The same specified harness, built and tested the same way each time, gives every machine's acceptance file the same shape, so a reviewer reads consistent evidence instead of a different shop-floor story per unit. How much that is worth depends on the volume and on how strict the customer's acceptance regime is.

What stays outside the harness is worth naming plainly. The PLC and control-cabinet design, the machine's process and hygienic zoning, and the validation of the finished machine remain with the OEM and its customer. What changes is the starting point: an assembled, tested harness with records, rather than a shop-floor build that has to be documented from scratch.

Talk to Our Engineers

If a food, beverage or pharmaceutical machine platform is at the stage where the harness approach is being decided, or a wash-capable variant is being standardised across frame sizes, that is the useful point to bring our harnessing specialists into the design and procurement conversation.

The details that shorten it are the harness drawing or schematic, the cleaning specification the machine has to meet, the agent, concentration, exposure and wash method, the connector and gland interfaces already fixed by the machine design, the expected build volume across variants, and the test records the customer's acceptance regime will ask for.

Talk to our harnessing specialists through the LAPP SEA enquiry page. LAPP engineers and produces both the cable and the connector, so the conversation can cover the run, the termination and the entry together. For application context, the machine and plant engineering channel covers the OEM and machine-builder side, and the food and beverage industry page covers the hygienic side.